Post Go back to editing

OpAmp with low common mode distortion

Category: Datasheet/Specs

We are looking for an op-amp to replace the input stage of a data acquisition instrument. Currently the front-end is an AD8510, configured as a non-inverting buffer. This frontend shall now be expanded with a 10:1 resistor divider to allow measuring higher input voltages. This attenuator however increases the source impedance as seen by the AD8510 to ~100kohms. We noticed a significant increase in THD:

A 10Vpk 1kHz sinewave connected without the attenuator (low source resistance, about 5k ohms) gives -105dB THD for the complete system, but the same signal connected via the attenuator results in -65dB THD. I assume this is caused by modulation of the op-amp input capacitance, which has no ill effect as long as the source resistance is small, but not so with a high source resistance.

Can you recommend a replacement for the AD8510 with low common mode distortion? The system constraints are:

single device
MSOP8 package
+/-15V operation
CM input range V+ - 2V, V- +2V or better
low voltage and current noise
low voltage and bias current offset
supply current less than 3mA

Many thanks, AK

  • Hello AK,

    May I know the application of your circuit? Also, can you send me your schematic? 

    Thank you!

    Regards, 

    Mae

  • Hello Mae,

    The application is a data acquisition frontend to measure sensors with an output voltage up to +/-12V with a bandwidth from DC up to 50kHz. The AD8510 is followed by a differential ADC driver (ADA7490) and an AD7768 ADC. The AD8510 operates as a run-of-the-mill non-inverting amplifier, either as a voltage follower or configured to a gain of 10.The input resistance should be as high as possible, minimum is 250K.

    There is a demand to measure higher input voltages which requires a passive pre-divider. First tests with a 200K - 220K divider (+/- a 24V input range) resulted in too high THD figures.

    Another option is implementing a 20:1 divider (380K - 20K) and using the x10 gain. This should significantly reduce the CM distortions but adds 20dB noise ...  So the preferred solution is a compatible op-amp with a low CM distortion figure.

    Best Regards, bdolf

  • Hi  ,

    We saw an alternative for your AD8510 that you could use in your system which is the ADA4610. However, the ADA4610-1 is only available in an 8-lead SOIC package and in a 5-lead SOT-23 package. The ADA4610-2 is the one available in 8-lead MSOP, 8-lead SOIC, and 8-lead LFCSP packages. 

    Hope this helps!

    Thank you!

    Best regards,

    Mae

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.