Post Go back to editing

AD8663

Category: Hardware
Product Number: AD8663

Hello,

AD8663 datasheet says operating voltage is 5 to 16V or +2,5/-2.5 to +8V/-8V.

I have been working on AD8663 supplying it from 3,3 volts (Vpos 3.3V Vneg 0V) without any problems.

Is this normal behaviour?

Regards

Parents
  • Hi  ,

    The AD8663 will only be able to operate for single supply withing the range of 5V to 16V and for dual supply, within the range of +/-2.5V to +/-8V. With that, I am suggesting to increase your supply to 5V (if you prefer a single supply) or maybe you could try having a -3.3V in your V- as well If the only available supply is 3.3V. 

    I hope this information helps.

    Thanks, 

    Mae

Reply
  • Hi  ,

    The AD8663 will only be able to operate for single supply withing the range of 5V to 16V and for dual supply, within the range of +/-2.5V to +/-8V. With that, I am suggesting to increase your supply to 5V (if you prefer a single supply) or maybe you could try having a -3.3V in your V- as well If the only available supply is 3.3V. 

    I hope this information helps.

    Thanks, 

    Mae

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.