Hi, I have question about the usage of disable pin of ADA4807 when using different powering.
In its datasheet page 25 : DISABLE CIRCUITRY, there is a graph and table to show threshold of disable pin.
if I use +/-3.3 supply for this amplifer, how to calculate the threshold of disable?
a. just care about the +Vs, then find the corresponding value below +Vs from graph Vth should be ~2V, then the Enable value is 3.3-1.85 = 1.45 V, Disable value is 3.3- 2.15 = 1.15V
b. calculate the +Vs-(-Vs) = 6.6V, then find the corresponding value below +Vs from graph Vth should be ~3.5V, then the Enable value is 3.3-3.35 = -0.05 V, Disable value is 3.3- 3.65 = -0.35V
which one is correct? please help answer this.
Thanks.