Hi
I’m using AD8062 by voltage follower. Then I have confirmed Vout drop from 3V to 2V.
Could you confirm the following specification.
V+ : 3.3V
V- : GND
+IN : 3V
Rload : none
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD8062
Production
The AD8061/AD8062/AD8063 are rail-to-rail output voltage feedback amplifiers offering ease of use and low cost. They have a bandwidth and slew rate typically...
Datasheet
AD8062 on Analog.com
AD8602
Production
The AD8601, AD8602, and AD8604 are single, dual, and quad rail-to-rail, input and output, single-supply amplifiers featuring very low offset voltage and...
Datasheet
AD8602 on Analog.com
Hi
I’m using AD8062 by voltage follower. Then I have confirmed Vout drop from 3V to 2V.
Could you confirm the following specification.
V+ : 3.3V
V- : GND
+IN : 3V
Rload : none
Hello,
Can you send me your circuit schematic for me to check?
Thanks.
Regards,
Paul
Hi
Thank you for quick reply.
Could you see the following.

Best Regards
Hello kshigemori281 ,
The input voltage range of AD8602 has a headroom of 1.8 V, meaning for it to work satisfactory, the input voltage should not exceed the Supply Voltage minus the headroom (Vs-headroom)
For example, for Vs = 5V, the input should not exceed +3.2 V
Max input voltage = Vs - headroom = 5V - 1.8V = 3.2V

In your schematic, using the above formula, the input voltage should not exceed 1.5 V for it to work satisfactory.
Max input voltage = Vs - headroom = 3.3V - 1.8V = 1.5V

As a recommendation, you can increase your supply voltage to 5V so the part can accept the 3V input and work as it intended to be.

Hi,
Thank you for quick reply.
I understood this reason!
Best Regards
Hello,
Glad that I can help!
Regards,
Paul