Hello.
When the AD8657 is output using a voltage follower, an output error that exceeds the specified offset voltage is confirmed.
The error range is roughly 30mV to 40mV. Since the specification is 16mV max., we cannot grasp the cause of this output error.
There is no external noise, etc., and the input is DC 1.8V.
What is the cause of the error?