Hello,
I am using AD8648 in a resistive load circuit where the input is a sinusoidal 2 VPP wave at 1 MHz, the dual supply is +3V and -3V. I firstly build the standard non-inverting amplifier circuit but it gave me high ringing and overshoot at the output, just to make sure the functioning of opamp, I switch the frequency to 1 KHz but still the ringing and overshoot was observed. I have also attached a 5pF compensating capacitor in series with the feedback resistor but still the same problem. Can anybody please enlighten the problems that I am facing, any help would be deeply appreciated.
Thank you in advance