Post Go back to editing

Amplifying signals from Piezo strip TE 10184000-01

Category: Hardware
Product Number: LTC2067 , ADA4051-2, AD8629

We are designing a device which would amplify the signals from a piezo strip TE 10184000-01. 

Earlier amplifier used was ADA4051-2 with average results to give the signals in the frequency band range of 0.2 to 05 Hz and 1 to 3 Hz.

Will the one out of the following two will be better?

LTC2067 ,

AD8629

We need minimum external components for the filtering of 50/60Hz and the above mentioned filtering of frequency signals. 



To get the signals from the piezo strip
[edited by: plawat at 3:43 AM (GMT -5) on 1 Dec 2022]