We are designing a device which would amplify the signals from a piezo strip TE 10184000-01.
Earlier amplifier used was ADA4051-2 with average results to give the signals in the frequency band range of 0.2 to 05 Hz and 1 to 3 Hz.
Will the one out of the following two will be better?
LTC2067 ,
AD8629
We need minimum external components for the filtering of 50/60Hz and the above mentioned filtering of frequency signals.
Edit Notes
To get the signals from the piezo strip[edited by: plawat at 3:43 AM (GMT -5) on 1 Dec 2022]