Post Go back to editing

LT1491 Voltage Rails

Category: Hardware
Product Number: LT1491

Hello, I have a question about the max voltage on the V+ and V- rails. Looking at the datasheet I see that V+ to V- has 44, so a bi-polar configuration would be +22V and -22V. Or a Positive only configuration would be V+ 44V and V- 0V. A Negative only configuration would be V- (-40V) and V+ 0V. Is that correct?

Thank you