Post Go back to editing

AD8392A Supply Pins

Thread Summary

The user asked about configuring the AD8392A in single supply mode. The support engineer clarified that Vee should be connected to the GND plane, and Vcc to the positive rail (≥10V). A stable +5V must be supplied to the IC-GND and used for Vcom (Fig. 18 in the datasheet).
AI Generated Content
Category: Hardware
Product Number: AD8392A

Hello everyone,

I want to build a simple non-inverting amplifier using AD8392A. I read the datasheet thoroughly that can be downloaded from here: https://www.analog.com/en/products/ad8392a.html?doc=AD8392A.pdf#product-overview

There are 3 pins related to the supply: Vcc, Vee and GND. If I want to use Single Supply mode, it is not clear to me based on the datasheet (because there is literally nothing written about it) that what to connect to Vee and GND? I suppose my positive rail goes to Vcc. Slight smile

Thank you for the help in advance