Hello,
On my previous design, I used LT1351 opamp not it is not availlable in the market. Do you recommend any other opamp with same features?
Thank you,
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LT1351
Production
The LT1351 is a low power, high speed, high slew rate operational amplifier with outstanding AC and DC performance. The LT1351 features lower supply current...
Datasheet
LT1351 on Analog.com
Hello,
On my previous design, I used LT1351 opamp not it is not availlable in the market. Do you recommend any other opamp with same features?
Thank you,
Hi AE104: that family has the same footprint in part number increments of 3. So for example LT1354 should work, also LT1357. The bandwidths and slew rates rise, so you'd want to double check stability.
Also, the LT1351 had a shutdown pin, which the others do not.
If your application is not using the high sew rate of the opamp, then there may be more alternatives.
Hi AE104: that family has the same footprint in part number increments of 3. So for example LT1354 should work, also LT1357. The bandwidths and slew rates rise, so you'd want to double check stability.
Also, the LT1351 had a shutdown pin, which the others do not.
If your application is not using the high sew rate of the opamp, then there may be more alternatives.