Post Go back to editing

Voltage Noise Spectrum Measurement Problems

Category: Hardware

At present, I have made a precise current source based on LT2057, ADA4870, and LT5400. I want to test the current noise spectral density of the entire system, so I want to use the constant current source output to connect the 1Ω load to test the voltage noise spectral density and realize it after conversion. I would like to ask how the measurement of voltage noise spectral density can be achieved? Do you use a spectrum analyzer? If possible, can Agilent E4402B/E4407B/7401A be implemented? Similar to such a result, thanks! 

 

At the same time, the simulation results of the whole board and current source based on LTspice are as follows:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.