Post Go back to editing

ADA4099-1 MULTIOUTPUT CURRENT SENSE

Category: Hardware
Product Number: ADA4099-1

Hi,

based on application circuit on fisrt page of ADA4099-1, i'm wondering if its possible to add another BSS123 to the current mirror to get a multi output (with different V/A sensitivity) by using the same OPAMP. Thanks

I saw a similar application in the Analog Dialog 48-04

Top Replies

Parents
  • Hi Nicola,

    I do not think that you can add anymore PMOS because in doing so, you will change the current on the output of the ADA4099-1 and therefore will also change the response of VOUT (different V/A value).

    What you can explore is to (1) utilize the VOUT of the application circuit and use it as the input to another circuit that will adjust the sensitivity, or (2) use a current mirror circuit but on the low side replacing the 1kohm resistor (see simplified circuit below). If you do (2) then you have to ensure that the effective resistance (Reff) on the low side is still 1kohm to maintain the 1V/A sensitivity at VOUT.  



    Hope it helps.

    Best Regards,
    Sham

Reply
  • Hi Nicola,

    I do not think that you can add anymore PMOS because in doing so, you will change the current on the output of the ADA4099-1 and therefore will also change the response of VOUT (different V/A value).

    What you can explore is to (1) utilize the VOUT of the application circuit and use it as the input to another circuit that will adjust the sensitivity, or (2) use a current mirror circuit but on the low side replacing the 1kohm resistor (see simplified circuit below). If you do (2) then you have to ensure that the effective resistance (Reff) on the low side is still 1kohm to maintain the 1V/A sensitivity at VOUT.  



    Hope it helps.

    Best Regards,
    Sham

Children