Will the +80V maximum input voltage still apply when the amplifier is not supplied?
Im currently working on a battery protection system where the ADA4099 is used to measure the current of the battery, however there can be cases where the battery is connected and the ADA4099 is not supplied (5V voltage regulator for the supply voltage is not connected to the battery). Is the ADA4099 still capable of 50V input voltage and 50V differential input voltage?
best regards
Peter