ADA4870
Recommended for New Designs
The ADA4870 is a unity gain stable, high speed current feedback amplifier capable of delivering 1 A of output current and 2500 V/μs slew rate from a 40...
Datasheet
ADA4870 on Analog.com
Hi
I had noticed ADA4870 being NRND.
Are there any replacement for this device?
Hi,
I moved this to the Operational Amplifiers community. Someone here should be able to help.
Hi WNAK,
Yes, ADA4870 is labeled as NRND.
The closest >1 Amp output current feedback (similar to ADA4870) device is LT1210 which can handle up to +/-15V supplies (vs. ADA4870 which can do 1 Amp output current with up to 40V total supply voltage).
Here are the specs for these parts in Excel for easy Filtering and viewing:
Regards,
Hooman
Hi WNAK,
Yes, ADA4870 is labeled as NRND.
The closest >1 Amp output current feedback (similar to ADA4870) device is LT1210 which can handle up to +/-15V supplies (vs. ADA4870 which can do 1 Amp output current with up to 40V total supply voltage).
Here are the specs for these parts in Excel for easy Filtering and viewing:
Regards,
Hooman