Post Go back to editing

LT1112 Saturating before expected

Category: Hardware
Product Number: LT1112

Hi!

I try to replace OPA2277 OpAmp for LT1112, mainly because I need more precise DC and offset behavior. The opamps are feeded with +-12Vdc. For OPA2277, and many others OpAmps tested, I can buffer voltages with +- 10V. With LT1112, when the positive voltage reaches aprox. +9V the output becames saturated. The negative side was OK.  The load is a 12KOhm resistor on both cases. The circuit is very simple, just a buffer with bypass capacitors close to the opamp. 

OPA2277, LF353 and AD706 work at the same condition, but LT1112 no.  

Any ideas???

Cristiano

  • Hi Cristiano,

    We are now reviewing your concern. 
    Is it correct to assume that you have checked it through actual evaluation of the parts? Or did you do it by simulation?
    Were you able to capture the important waveforms?
    We would appreciate if you could share them with us.

    Thank you!
    Sham