Post Go back to editing

LT1782 short circuit protection

Category: Hardware
Product Number: LT1782

Hello,

I am evaluating if the LT1782 has short circuit protection or not.

Looking at the circuit diagram from its datasheet, it seems to me that the output stage HAS NOT a short circuit protection circuit.

Also, the datasheet does not mention nothing about it.

Could you confirm ?

Thanks,

Simon

  • Hi,

    It is a simplified schematic, so does not contain all of the components. The datasheet specifies the short-circuit current, so the part limits the output current. Don't forget to read the related note about heat dissipation. In the absolute maximum ratings table you can also see a statement: 'Output Short-Circuit Duration: Indefinite'. However, the heat dissipation should be kept within the specifications, as note 2 says ('A heat sink may be required to keep the junction temperature
    below absolute maximum.').