Post Go back to editing

AD8022 Spice Noise Model

Category: Software
Product Number: AD8022

Is there an update for the AD8022 spice model that fixes the noise? The model on the website shows the opamp having hundred's of nV per rtHz noise. This issue was brought up in 2017:  AD8022 spice model noise problem but it seems the spice model on the website has not been updated (last update 2012).

Also, tried the spice model attached in that forum post, it has much lower noise, but too low. With the op-amp as a unity gain buffer and a ground for the plus pin input, I get 1nV/rtHz of noise but the datasheet has 2.5nV/rtHz.

Thanks,

Ben

  • Hi, 

    We'll check the model and get back to you.

  • Hi Ben, 

    I ran a simulation using the model attached in the forum for VS=+/-12V and VS=+/-2.5V and got 2.30nV/rtHz at f=100kHz. Can you share the simulator and circuit used? 

    Thanks, 

    Gerdan

  • No problem. Attached is my .asc for the LTSpice sim. For some reason it won't let me upload the .asy file I'm using for the ad8022, so I've put it inline as code:

    Version 4
    SymbolType CELL
    LINE Normal -32 32 32 64
    LINE Normal -32 96 32 64
    LINE Normal -32 32 -32 96
    LINE Normal -28 48 -20 48
    LINE Normal -28 80 -20 80
    LINE Normal -24 84 -24 76
    LINE Normal 0 32 0 48
    LINE Normal 0 96 0 80
    LINE Normal 4 44 12 44
    LINE Normal 8 40 8 48
    LINE Normal 4 84 12 84
    LINE Normal 20 84 12 84
    LINE Normal 16 72 16 80
    WINDOW 0 16 32 Left 2
    WINDOW 3 16 96 Left 2
    SYMATTR Value AD8022
    SYMATTR Prefix X
    SYMATTR ModelFile ad8022b.cir
    PIN -32 80 NONE 0
    PINATTR PinName 100
    PINATTR SpiceOrder 1
    PIN -32 48 NONE 0
    PINATTR PinName 101
    PINATTR SpiceOrder 2
    PIN 0 32 NONE 0
    PINATTR PinName 102
    PINATTR SpiceOrder 3
    PIN 0 96 NONE 0
    PINATTR PinName 103
    PINATTR SpiceOrder 4
    PIN 32 64 NONE 0
    PINATTR PinName 104
    PINATTR SpiceOrder 5
    PIN 16 96 NONE 0
    PINATTR PinName 106
    PINATTR SpiceOrder 6

    AD8022Test.asc

  • Hi Ben, 

    Re-created your test using the .cir from the forum and still got 2.3nV/rtHz. I noticed that the referenced model file in the code is  .

    I've attached the .cir from the forum here. Can you try using this model instead?

    *AD8022 Macro-model
    *Function:Amplifier
    *
    *Revision History:
    *Rev.2.1 Feb 2017-ZZ
    *Copyright 2017 by Analog Devices
    *
    *Refer to http://www.analog.com/Analog_Root/static/techSupport/designTools/spicemodels/license
    *for License Statement. Use of this model indicates your acceptance
    *of the terms and provisions in the License Staement.
    *
    *Tested on MultSIm, SiMetrix(NGSpice), PSpice
    *
    *Not modeled: Distortion, PSRR, Overload Recovery,
    *             Shutdown Turn On/Turn Off time
    *
    *Parameters modeled include:
    *   Vos, Ibias, Input CM limits and Typ output voltge swing over full supply range,
    *   Open Loop Gain & Phase, Slew Rate, Output current limits, Voltage & Current Noise over temp,
    *   Capacitive load drive, Quiescent and dynamic supply currents,
    *   Shut Down pin functionality where applicable,
    *   Single supply & offset supply functionality.
    *
    *Node Assignments
    *               Non-Inverting Input
    *               |   Inverting Input
    *               |   |   Positive supply
    *               |   |   |   Negative supply
    *               |   |   |   |   Output
    *               |   |   |   |   |
    .Subckt AD8022 100 101 102 103 104
    *
    ***Power Supplies***
    Rz1	102	1020	Rideal	1e-6
    Rz2	103	1030	Rideal	1e-6
    Ibias	1020	1030	dc	0.4e-3
    DzPS	98	1020	diode
    Iquies	1020	98	dc	3.6e-3
    S1	98	1030	106	113	Switch
    R1	1020	99	Rideal	1e7
    R2	99	1030	Rideal	1e7
    e1	111	110	1020	110	1
    e2	110	112	110	1030	1
    e3	110	0	99	0	1
    *
    *
    ***Inputs***
    S2	1	100	106	113	Switch
    S3	9	101	106	113	Switch
    VOS	1	2	dc	1.5e-3
    IbiasP	110	2	dc	2.5e-6
    IbiasN	110	9	dc	2.5e-6
    RinCMP	110	2	Rideal	7e6
    RinCMN	9	110	Rideal	7e6
    CinCMP	110	2	0.8e-12
    CinCMN	9	110	0.8e-12
    IOS	9	2	0.12e-6
    RinDiff	9	2	Rideal	20e3
    CinDiff	9	2	0.8e-12
    *
    *
    ***Non-Inverting Input with Clamp***
    g1	3	110	110	2	0.001
    RInP	3	110	Rideal	1e3
    RX1	40	3	Rideal	0.001
    DInP	40	41	diode
    DInN	42	40	diode
    VinP	111	41	dc	0.71
    VinN	42	112	dc	1.21
    *
    *
    ***Vnoise***
    hVn	6	5	Vmeas1	707.10678
    Vmeas1	20	110	DC	0
    Vvn	21	110	dc	0.65
    Dvn	21	20	DVnoisy
    hVn1	6	7	Vmeas2	707.10678
    Vmeas2	22	110	dc	0
    Vvn1	23	110	dc	0.65
    Dvn1	23	22	DVnoisy
    *
    *
    ***Inoise***
    FnIN	9	110	Vmeas3	0.7071068
    Vmeas3	51	110	dc	0
    VnIN	50	110	dc	0.65
    DnIN	50	51	DINnoisy
    FnIN1	110	9	Vmeas4	0.7071068
    Vmeas4	53	110	dc	0
    VnIN1	52	110	dc	0.65
    DnIN1	52	53	DINnoisy
    *
    FnIP	2	110	Vmeas5	0.7071068
    Vmeas5	31	110	dc	0
    VnIP	30	110	dc	0.65
    DnIP	30	31	DIPnoisy
    FnIP1	110	2	Vmeas6	0.7071068
    Vmeas6	33	110	dc	0
    VnIP1	32	110	dc	0.65
    DnIP1	32	33	DIPnoisy
    *
    *
    ***CMRR***
    RcmrrP	3	10	Rideal	1e12
    RcmrrN	10	9	Rideal	1e12
    g10	11	110	10	110	-1e-10
    Lcmrr	11	12	1e-12
    Rcmrr	12	110	Rideal	1e3
    e4	5	3	11	110	1
    *
    *
    ***Power Down***
    VPD	111	80	dc	2
    VPD1	81	0	dc	1.5
    RPD	111	106	Rideal	0.286e6
    ePD	80	113	82	0	1
    RDP1	82	0	Rideal	1e3
    CPD	82	0	1e-10
    S5	81	82	83	113	Switch
    CDP1	83	0	1e-12
    RPD2	106	83	1e6
    *
    *
    ***Feedback Pin***
    *RF	105	104	Rideal	0.001
    *
    *
    ***VFB Stage***
    g200	200	110	7	9	1
    R200	200	110	Rideal	250
    DzSlewP	201	200	DzSlewP
    DzSlewN	201	110	DzSlewN
    *
    *
    ***Dominant Pole at 26 Hz***
    g210	210	110	200	110	2.6014e-6
    R210	210	110	Rideal	6.12e6
    C210	210	110	1e-012
    *
    *
    ***Output Voltage Clamp-1***
    RX2	60	210	Rideal	0.001
    DzVoutP	61	60	DzVoutP
    DzVoutN	60	62	DzVoutN
    DVoutP	61	63	diode
    DVoutN	64	62	diode
    VoutP	65	63	dc	6.997
    VoutN	64	66	dc	6.997
    e60	65	110	111	110	1.052
    e61	66	110	112	110	1.052
    *
    *
    ***Pole at 88MHz***
    g220	220	110	210	110	0.001
    R220	220	110	Rideal	1000
    C220	220	110	1.8086e-12
    *
    ***Buffer***
    g230	230	110	220	110	0.001
    R230	230	110	Rideal	1000
    *
    ***Buffer***
    g240	240	110	230	110	0.001
    R240	240	110	Rideal	1000
    *
    ***Buffer***
    g245	245	110	240	110	0.001
    R245	245	110	Rideal	1000
    *
    ***Buffer***
    g250	250	110	245	110	0.001
    R250	250	110	Rideal	1000
    *
    ***Buffer***
    g255	255	110	250	110	0.001
    R255	255	110	Rideal	1000
    *
    ***Buffer***
    g260	260	110	255	110	0.001
    R260	260	110	Rideal	1000
    *
    ***Buffer***
    g265	265	110	260	110	0.001
    R265	265	110	Rideal	1000
    *
    ***Buffer***
    g270	270	110	265	110	0.001
    R270	270	110	Rideal	1000
    *
    ***Buffer***
    e280	280	110	270	110	1
    R280	280	285	Rideal	10
    *
    ***Peak: f=360MHz, Zeta=1.8, Gain=15dB***
    e290	290	110	285	110	1
    R290	290	292	Rideal	10
    L290	290	291	1.228e-9
    C290	291	292	159.155e-12
    R291	292	110	Rideal	2.163
    e295	295	110	292	110	5.6234
    *
    *
    ***Output Stage***
    g300	300	110	295	110	0.001
    R300	300	110	Rideal	1000
    e301	301	110	300	110	1
    Rout	302	303	Rideal	 26
    Lout	303	310	 3e-9
    Cout	310	110	 6.3e-12
    *
    *
    ***Output Current Limit***
    H1	301	304	Vsense1	100
    Vsense1	301	302	dc	0
    VIoutP	305	304	dc	9.336
    VIoutN	304	306	dc	9.336
    DIoutP	307	305	diode
    DIoutN	306	307	diode
    Rx3	307	300	Rideal	0.001
    *
    *
    ***Output Clamp-2***
    VoutP1	111	73	dc	2.085
    VoutN1	74	112	dc	2.085
    DVoutP1	75	73	diode
    DVoutN1	74	75	diode
    RX4	75	310	Rideal	0.001
    *
    *
    ***Supply Currents***
    FIoVcc	314	110	Vmeas8	1
    Vmeas8	310	311	dc	0
    R314	110	314	Rideal	1e9
    DzOVcc	110	314	diode
    DOVcc	102	314	diode
    RX5	311	312	Rideal	0.001
    FIoVee	315	110	Vmeas9	1
    Vmeas9	312	313	dc	0
    R315	315	110	Rideal	1e9
    DzOVee	315	110	diode
    DOVee	315	103	diode
    *
    *
    ***Output Switch***
    S4	104	313	106	113	Switch
    *
    *
    *** Common Models ***
    .model	diode	d(bv=100)
    .model	Switch	vswitch(Von=1.505,Voff=1.495,ron=0.001,roff=1e6)
    .model	DzVoutP	D(BV=4.3)
    .model	DzVoutN	D(BV=4.3)
    .model	DzSlewP	D(BV=19.696)
    .model	DzSlewN	D(BV=19.696)
    .model	DVnoisy	D(IS=1.95e-16 KF=9.99e-16)
    .model	DINnoisy	D(IS=5.42e-17 KF=4.45e-16)
    .model	DIPnoisy	D(IS=5.42e-17 KF=4.45e-16)
    .model	Rideal	res(T_ABS=-273)
    *
    .ends
    

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.