Hello
I have a question about applying voltage to the output terminal of ADA4857-2.
Is there a risk of damage to the IC when used under the following conditions?
・ Power supply voltage: + 5V / 0V
・ PD terminal: High (PowerDown)
・ Input: No input
・ Output terminal: 1Vp-p sine wave applied
If the PD terminal is set to High, will the voltage be applied to the output terminal when the power supply voltage is cut off?
I would be grateful if you could reply.
Best Regards,
Knj