Category: Hardware
Product Number: LT1970a with nA current limit set
Hi!
I'm using the LT1970a in current limit mode (sink and source).
I replaced the shunt current monitor resistor (RCS) of the evaluation board of the LT1970a : DC453B-A with a set (20, 200, 2k, 20k) in order to work at different current range.
Which is the best strategy to move to nA range?
It seems that +/- 4mV is the lowest limit SENSE+/- input stage:
I was thinking to add INA amplifier between shunt resistor RCS and SENSE+/- pin.
Thanks in advance for any comments!