why?
AD8032
Production
The AD8032 (dual) is a single supply voltage feedback amplifier that features high speed performance with 80 MHz of small signal bandwidth, 30 V/µs slew...
Datasheet
AD8032 on Analog.com
Hi,
You may want to check the Files from Get Files tab under Next Steps. It directly translates the circuit from the tool to LTSpice where you can simulate. It also provides not just the circuit but also the guide for different analysis and simulations. You may want to try using LTSpice.
Below is where you can download the files and a sample of AC Analysis included. If it still doesn't work, you may share your .json file from the tool and I can have a look. Thanks!