Post Go back to editing

LTC6560

How to check that LTC6560 is properly grounded via thermal pad? I put one pull down resistor-60Kohm to input (Din), but the voltage at this pin is still showing is 1.5 Volt !!! I am using this IC for APD with positive bias. (equal to Vref-pin of IC), please suggest.

  • Hi ,

    The LTC6560 input is biased to 1.5V nominal internally when Active:

    So, you're measuring a valid input voltage. At least electrically, it seems like the exposed pad is properly grounded.

    Also, from datasheet page 14:

    "To maximize dynamic range, the LTC6560’s input is limited
    to negative current pulses (current flowing out of
    the LTC6560). When using a negatively biased APD, the
    TIA input can be AC or DC coupled to the APD cathode.
    When using a positively biased APD, the input must be
    AC coupled to the APD’s anode."

    Let me know if you have any quesitons.

    Regards,

    Hooman

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.