Post Go back to editing

high output current opamp (AD8531)

Hi,

I‘m trying to find a opamp with high output current (>100mA) used as voltage follower to drive a RLC circuit. The driving signal is around 900kHz, ±1.5V.  Currently I'm working on AD8531 and only have ±3V power supply for the opamp. And in the datasheet it's said the AD8531 shall only work with single opreation supply and the range is 6V. I don't think ±3V is good for it but I'm not so sure. (As I understand all the opamp can work under dual supply range). So I can find a OPAMP which can output 900kHz ,±1.5V(or more)  and  >100mA output current and operating at ±3V? Or is there any other simple design?

Many thanks!

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.