Post Go back to editing

Which is an alternative to the LTC6268 for 10 V operation?

Hi,

I want to implement a simple peak detector with a precision diode. I am using the LTC6268-10 to implement the >10 MHz precision diode due to its low input capacitance. However, I would like to increase the voltage supply to +-5V. Thus, I am looking for an amplifier with >100 MHz BW, >10 V/us SR, Vdd-Vss >= 10 V, and low input capacitance (comparable to LTC6268-10). Which one should I choose?

Thanks in advance.

Edit Notes

Corrected some typos.
[edited by: dpalma at 9:04 AM (GMT -5) on 18 Nov 2021]