Hi,
I am using only one OPA within LT1254 (the connection was tested in LT Spice enviroment and was working there). For the remaining 3 OPAs I connected + to GND, - and OUT together with a 620E resistor. The + IN of used OPA is driven with either + or - 4.5V, while the rail voltages are +10V and -5V. The rail current limitation used is 100mA causes the positive rail to drop to 4V. The chip operating temperature during testing is 35°C.
Do you have any idea what would be the issue for such a consumption?
Best regards,
Anja