Dear Team,
May I know the Typ offset voltage of AD8531.In the datasheet, only the Max value is given.
I am using AD8531 as a unity gain buffer with a single supply of 5V

Regards
HARI
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
November Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Ever wonder how EMC limits came to be and why they matter? Dive into the interesting bits of EMC limits and levels, then test your knowledge with EMC: The Interesting Bits Quiz.
Read the blog first: EMC Limits and Levels Explained: Well, the Interesting
View All
AD8531
Production
The AD8531, AD8532 and AD8534 are single, dual and quad rail-to-rail input and output single-supply amplifiers featuring 250 mA output drive current. This...
Datasheet
AD8531 on Analog.com
Dear Team,
May I know the Typ offset voltage of AD8531.In the datasheet, only the Max value is given.
I am using AD8531 as a unity gain buffer with a single supply of 5V

Regards
HARI
Hi Hari,
You can check AD8531's typical offset voltage in the Typical Characteristic Performance section in the datasheet page 6 figure 6 and 7. For your application of 5V supply, typical input offset voltage of AD8531 is along -6 to -4mV. Kindly see image below:

Hope this helps!
Regards,
Kristine
Hi Kristine,
Thank you very much.
I saw this curve, but I don't know how to interpret this curve.
The X-axis is offset voltage Y-axis is quantity.
If you don't mind could you please tell me how you get that range( -6 to -4mV)
Regards
HARI
Hi Hari,
We interpret this data by looking at the highest number of units and see what the offset voltage of that said no. of units. In this graph, the highest number of units which is more than 500 unit's offset voltage were ranging -6mV to -4mV. This shows that the typical(usual) offset voltage of this generic is around that range -6 to -4mV.

Hope this helps.
Regards,
Kristine
Hi Kristine,
Thank you very much. That is very informative.
One more question I have when I am stimulating a buffer using AD8531,output voltage is always 3mv less than expected.I don't know whether it is an issue with the spice model or not.
May I know why

Regards
HARI