Hi engineers,
May I know what is the maximum amount of attenuation I can get by using the LT1128 and is there any op amp that is recommended for attenuation? I am looking to create an -60dB attenuator for signals in low frequency (around 500hz) with low electronic noise and I was wondering if I could do it by cascading 3 -20dB active attenuator (close loop inverting amplifier where where gain = -r2/r1 and r1>r2) together. I understand that I might be missing some key information here but I would appreciate any comments or suggestions that can get me started as I am still fairly new in this field.
Rgds,
Hong
Edit Notes
added some information[edited by: hong_96 at 9:57 AM (GMT -4) on 23 Aug 2021]