Hello everyone,
can I use the AD8604 in an environment with two power supplies? E.g. -3V3 and +3V3?
Thanks in advance
Andreas
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
AD8604
Production
The AD8601, AD8602, and AD8604 are single, dual, and quad rail-to-rail, input and output, single-supply amplifiers featuring very low offset voltage and...
Datasheet
AD8604 on Analog.com
Hello everyone,
can I use the AD8604 in an environment with two power supplies? E.g. -3V3 and +3V3?
Thanks in advance
Andreas
Hi Andreas,
AD8604 can work with dual supply provided that it’s total supply span/range is less than its absolute maximum rating of 6V, to ensure proper functionality and device reliability. In your case, if you will use -3.3V/+3.3V, that is equivalent to a 6.6V supply range and you will violate the Abs Max Rating and would not guarantee the product’s performance, functionality and reliability. For optimum device performance, it is recommended to use 2.7V to 5V single supply or equivalent of +/-1.35V to +/-2.5V in dual supply. Hope this helps.
Oh yes. Thank you very much.