Post Go back to editing

LT1819 not responding

In simulation LT1819 is working at -3V to +9V, but in actual is not working. Another issue is if I connect 0 to 5V also It is not responding. Can you please help on this

Parents Reply
  • Hi,

    Since you are also seeing oscillation as you have mentioned (-200mV to 500mV), please consider using feedback capacitor along with your feedback resistor (R3) at U1.
    The Cf value is obtained by the equation: CF > RG • CIN/RF

    Also, the U2 is driving 10nF Cap load.
    Please use isolation resistor value of 10 to 50 ohms as recommended by the data sheet.

    And the least thing, if you are open on using fresh unit to check if you will have the same performance as what you have now.
    In addition, please use supply voltage of 10V only.

    Thanks and regards!

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.