Post Go back to editing

LT1819 not responding

In simulation LT1819 is working at -3V to +9V, but in actual is not working. Another issue is if I connect 0 to 5V also It is not responding. Can you please help on this

Parents Reply
  • Hello,

    The part was specified at +/-5V (10V).
    We can guarantee device performance using this supply range.

    Using supply of -3V to 9V means 12V supply range.
    The device Absolute Maximum Rating is 12.6V.
    Any overshoot on your voltage supply will possible hit and violate Abs Max Rating.

    Hence, the PSRR of the part is tested up to 11V only.

    Can you do a diode check on the LT1819 pins?
    This to check for any shorted pins.

    Thanks and regards!

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.