Hi,
in a scenario where I want to use the LT1818 (output stage of scope differential probe) it can happen that the inputs stay at a differential voltage of about 4V for longer (when a wrong attenuation is selected or to high signal is measured). The inputs however always stay within V+ and V-. In front of the inputs are 100Ohm resistors. Amp runs in Gain 11 config (1k feedback). LTspice shows input currents in the range of under 10µA. The datasheet says to avoid this scenario because the amp may draw excessive current in the range of 50mA; however LTspice shows only 7.3mA and 13mA at +/-5V (output is 1Meg loaded). Is the simulation simplified there and doesn't show the excessive current draw problem, or is there no inherent danger of damage in my scenario?
Thanks,
Simon