Post Go back to editing

AD8047 problem

Hi ,

Im using AD9744 DAC for one of my project and AD8047 for I_V converter for that DAC. Im getting output voltage twice the Input to adc fron AD8047.

Can anyone tell me how to connect onli one OUTA to AD8047.

Regards,

Bhavya

SCHEMATIC156.pdf
Parents
  • Bhavya,

    The  AD9744 converts input digital word to differential current outputs at IOUTA and IOUTB. These currents are converted to voltages across R410 & R411. This differential voltage is fed as input to differential amplifier AD8047.

    The gain of the amplifier is decided by ratio (R404/R405. R409 = R404 and R406 = R405). At present it is 500E/225E = 2.2222, which is why you are getting doubled output. In case you need 1:1 output, you will have to replace R404, R405, R406 and R409 by equal value resistors.

    The op amp output DAC2_VOUT is single ended with respect to analog ground.

    Hope this helps.

    Regards,

    JayantD

  • Why is the output  voltage  value of  AD9744 decided by R410 & R411?? Don't they just decide the currents of AD9744??

Reply Children
No Data