Post Go back to editing

Heat problem in AD811ANZ

Hello all,

    I am using AD811 in my amplifier circuit.In this circuit ,I am giving 1V sine ,triangular and square wave signal at 10Hz to2MHz  to the input of amplifier.If I  use this IC ,over a  long period of time ,it produce the heat on the surface of the IC.Eventhough I got a good  output response form this IC .If  I use this IC continuously  the heat problem completely affect the IC of  functionality and it will lead to IC dead.

Hereby, I attached the my amplifer circuit for your reference.

Please suggest the good solution for this problem.

Thanks with Regards,

Newengg

Parents
  • Thanks for your reply,

    I didn't get the oscillating output response throughout the whole testing process ;Please explain the matter of LM324.I didn't get your point regarding of LM324.

    Is it necessary to add the 10uF with +/- 15 V of LM324?

    Should the LM 324 eliminate  from the amplifier circuit?

    Regards,

    Newengg

Reply
  • Thanks for your reply,

    I didn't get the oscillating output response throughout the whole testing process ;Please explain the matter of LM324.I didn't get your point regarding of LM324.

    Is it necessary to add the 10uF with +/- 15 V of LM324?

    Should the LM 324 eliminate  from the amplifier circuit?

    Regards,

    Newengg

Children
No Data