Using AD8561 for 100kHz or higher frequency Sine to Square Wave Conversion (zero crossing detector)

Hi, I have a question about using AD8561 for 100kHz or higher frequency Sine to Square Wave Conversion.

The comparator I'm using is AD8561 and the circuit diagram I set up on breadboard is

Inline image 1

And the response I get is as follows, with sine wave as input and blue as pin7 output.

Is there a way to get rid of these ripple/oscillation and get 7ns response bandwidth? 

Inline image 2

Inline image 3

Inline image 4

Is there a way to get rid of these ripple/oscillation and get 7ns response bandwidth?