Good afternoon. I have a customer considering the use of the ADA4800 (Low Power, High Speed CCD Buffer Amplifier) with one of the ADI AFEs. The data sheet only indicates the "typical" output voltage noise at a frequency of 20MHz. Do you have a graph showing a more complete picture of this parameter over then entire 400MHz potential bandwidth that I can send to the customer?
Thank you.
Rich