Post Go back to editing

Boosting AD8642 output current

I'm testing a design in which I need to do a current to voltage conversion. The current ranges from picoamperes to 100mA (both positive and negative), so I use 4 different resistors and a switch to select each of them. I filter the corresponding signal (not shown in the image), use a variable gain (x1, x10, x100, x1000) amplifier and then adapt it and detect it. 

Everything works perfectly fine till 20mA, the op amp output current limit. Can anyone please show me a simple power stage that can be used preferibly inside the feedback loop? The output voltage has to be between -5 and +5 volts and has to work for +-100mA.

Parents
  • Hi Damaso,

    Thanks for using ADI products on your application. If replacing the AD8642 with another opamp that has a higher output drive capability is not an option for you then you can try to implement the circuit below.

    There are other power/current booster design circuits on the internet which you can also consider and implement.

    Also, I noticed from your schematic that there is a short between the output pin of U2 and the negative supply. I would recommend that you avoid this in your actual circuit

    I hope this helps!

    Best regards,

    Emman

Reply
  • Hi Damaso,

    Thanks for using ADI products on your application. If replacing the AD8642 with another opamp that has a higher output drive capability is not an option for you then you can try to implement the circuit below.

    There are other power/current booster design circuits on the internet which you can also consider and implement.

    Also, I noticed from your schematic that there is a short between the output pin of U2 and the negative supply. I would recommend that you avoid this in your actual circuit

    I hope this helps!

    Best regards,

    Emman

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.