1.can any one tell me which is the better one. LM124 or OP467?or any other quad opamp?
2. can any body suggest a replacement for ISO120 isolation amplifier?
OP467
Production
The OP467 is a quad, high speed, precision operational amplifier. It offers the performance of a high speed op amp combined with the advantages of a precision...
Datasheet
OP467 on Analog.com
1.can any one tell me which is the better one. LM124 or OP467?or any other quad opamp?
2. can any body suggest a replacement for ISO120 isolation amplifier?
i am currently using LM747 in my design. so i want an opamp which is
1. comparable or better in performance to 747
2. quad
3. mil grade
what do u think of LM124 and op467. how do u compare them?
if mil grade isolation amplifier is not available, what are the other options?
i am currently using LM747 in my design. so i want an opamp which is
1. comparable or better in performance to 747
2. quad
3. mil grade
what do u think of LM124 and op467. how do u compare them?
if mil grade isolation amplifier is not available, what are the other options?