Amp01 single 9V battery supply ... problems

I am using an Amp01 as a simple 200X (V/V) Op-Amp in a portable situation with a single 9V battery.

The amp circuit is as described in the data sheets, with the 1K & 10K resistors, however a single 9V battery is being used with the battery ground created with two 100K resistors each connected to a battery terminal & the common ends of these resistors connected to the Amp01 ground & pin 8(Reference). The amp works fine, but the battery life is far less than the expected two months: A fresh 9V battery(9.31V unloaded) will drop down to 8.54V within 24 hrs, and down to 6.45V within 10 days. This current draw seems too high{ for the stated ~3mA of the Amp01} and clearly it appears that excess current may be flowing through the Amp01 via substrate paths(diode & transistor). Is there a better way to power this amp via a single 9V cell ?

thanks

Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 2:35 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 2:35 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data