ADA4870 Die Temperature Monitor

Can I use the Thermal Monitor and Short-Circuit Flag (TFL) pin to monitor peak die temperature?

  • 0
    •  Analog Employees 
    on Aug 5, 2014 7:11 PM

    Hello,

    Good question, given there are process variations with the ADA4870 and semiconductors in general, this prevents the TFL pin from being used as an indicator of absolute die temperature. However, the TFL pin can be used to monitor relative changes in the die temperature. The voltage on the TFL pin varies at approximately -3mV/C.

    I hope this helps.

    Regards

    John

  • 0
    •  Analog Employees 
    on Aug 2, 2018 2:44 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin