OP296 input resistance

Hi, i would like to know the OP296 input resistance. I was wondering if the OP296 works as a transimpedance amplifier with a 1M feedback resistance (so i need that value). any advice?.


And the same question for ADA4528.

Thanks.

Parents
  • Hello,

    the worst case input bias current of the OP296 is +-50nA, which you have to add or deduct from the current of your source (a photodiode, for example). Say, your photodiode sources 500nA then you expect 0.5V at the output of your opamp. In a worst case situation you will only get 0.45V or even 0.55V.

    The input offset current is not included in the calculation.

    Best regards,

    Reinhard

Reply
  • Hello,

    the worst case input bias current of the OP296 is +-50nA, which you have to add or deduct from the current of your source (a photodiode, for example). Say, your photodiode sources 500nA then you expect 0.5V at the output of your opamp. In a worst case situation you will only get 0.45V or even 0.55V.

    The input offset current is not included in the calculation.

    Best regards,

    Reinhard

Children
No Data