AD8036: need clarification on "fast rectifier" use.

First a disclaimer, I'm only a mechanical engineer, doing this out of necessity as a grad student.

I'm hoping to use either AD8036 or AD8037 as a peak detector for a nearly sinusoidal waveform at 100Hz-5MHz. The datasheet gives this handy schematic on page 19 and claims good performance to 20MHz. I am willing to tolerate error of a couple % at high frequency.

However, the same datasheet also says on page 16 (bottom of right column) that "The AD8036's and AD8037's CLAMPIN input clamp architecture works only for noninverting or follower applications..."

Doesn't the schematic show an inverting application?  Is this just an "oops" or is it the correct layout?


Now just a couple of basic questions. My intent is to use a simple RC filter on the output. I am sampling the output at 10Hz so a large time constant is desired. Can I assume that in this case, a relatively large C (0.1uF) does not constitute a problematic capacitive load?

Thanks!

Top Replies

Parents
  • 0
    •  Analog Employees 
    on Sep 20, 2014 11:32 PM

    Hi Ilya,

    Sorry for the delayed response.

         1. First, the datasheet theory of operation (pg. 15, paragraph 2) says that AD8036 and AD8037 can be used in either inverting or non inverting configuration but the clamp in function will only work at non inverting mode. in conjunction to this, Application Section (pg 17) says that the clamping feature of AD8036 and AD8037 only works when the amplifier is configured in non inverting mode, but to clamp in an inverting circuit an additional inverting gain stage is needed. With the circuit in Figure 12, these restrictions are met.

          With your concern 'does follower in this case means unity gain inverting?', Yes you're right but for the case when the input is in negative cycle only. For the positive input cycle, the operation is different (the operation explained on page 19).

         2. Can you share to me the circuit you have in mind? I want to have a closer look to assist you better. Thanks.

    Best Regards,

    Jino

Reply
  • 0
    •  Analog Employees 
    on Sep 20, 2014 11:32 PM

    Hi Ilya,

    Sorry for the delayed response.

         1. First, the datasheet theory of operation (pg. 15, paragraph 2) says that AD8036 and AD8037 can be used in either inverting or non inverting configuration but the clamp in function will only work at non inverting mode. in conjunction to this, Application Section (pg 17) says that the clamping feature of AD8036 and AD8037 only works when the amplifier is configured in non inverting mode, but to clamp in an inverting circuit an additional inverting gain stage is needed. With the circuit in Figure 12, these restrictions are met.

          With your concern 'does follower in this case means unity gain inverting?', Yes you're right but for the case when the input is in negative cycle only. For the positive input cycle, the operation is different (the operation explained on page 19).

         2. Can you share to me the circuit you have in mind? I want to have a closer look to assist you better. Thanks.

    Best Regards,

    Jino

Children
No Data