Post Go back to editing

AD8512 Half-Wave and Full-Wave Rectifiers

It was produced in the p16 of the data sheet "Half-Wave and Full-Wave Rectifiers" circuit uses the AD8512 our customers.

It is the output level of the output signal is different.
I will attach the output waveform.

Why level or probably would be different?
In addition, the What is the cause?

Regards,
Yuji

AD8512_Waveform.pdf
  • Hello Yuji,

    positive input signals are well accepted, as you use +15V supply.

    Negative input signals are cut, as you use 0V for the negative supply,

    but there will be some dropout voltage.

    Maybe this is the reason for it.

    Regards,

  • Hi Yuri,

    I'm still figuring out what should cause the change in the output voltage level.Maybe r.daemon is right but it should came out as what is shown on the data sheet. I'll get back to you soon.

    Regards,

    Philip

  • Hello r.daemon,

    Thank you for information.

    Do you not the same as the data sheet, if as of the information?

    Is there a way to output the same level in this rectifier circuit?

    Regards,

  • Hi Yuri,

    In theory, it should work with ideal amplifiers but due to the inherent offset of the amplifiers and the gain of the circuit the output will not be perfect. The device doesn't really rail to the ground during the negative half cycle. So, base on this equation during the negative half cycle: Vout= (1+R7/R2)Vo -(R7/R2)Vin, where Vo is the output of the first stage and supposedly zero/ground but is not and is being amplified by gain of (1+R7/R2) which is not present during the positive half cycle of your input causes that difference in the out level of the circuit.

    On the other hand, may I ask how your costumer measures the output based on the screenshot, the output voltage is 200mv while the input is 2V. do use something to attenuate the signal?

    Regards,

    Phil

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin