Queries about AD8099

Dear Supporter,

I have a query about AD8099. I use AD8099 in my product. The package is SOIC-8.

The power supply is +/-5V. The gain is set as -10.

Input signal is square wave with the frequency of 2MHz.

After increasing the input amplitude, the output gets its full range.

The output has over-shoot. My schematic and testing results are attached for your reference.

I tested with signal generator and oscilloscope, which means the output doesn’t have capacitive load. We used AD817 and AD847 before, AD817 and AD847 worked well.

I have two queries here.

1, why is there over-shoot here? How can I eliminate it?

2, I read the description of Pin Cc in the datasheet. It is used as compensation for the gain range of –1, +2 to +10. Is it worked for the gain of -10? Is it the over-shoot caused by the poor compensation work design?

Could you please help give some comments on the issues?

Thanks in advance for your help and support!

Br,

Wayne

attachments.zip
Parents Reply Children
No Data