Post Go back to editing

using AD8067 as inverting amplifier

Hi,

I tried to work with AD8067 operational amplifier as inverting amplifier. My input resistance is 12k ohm and feedback resistance is 10k ohm. Now gain should be less than one. I tried to simulate it in LTspice with spice model of AD8067 from analog device website. I got very weird result. The frequency increased and the output is like a beam. I am attaching the circuit and output curve here. Can anyone please help me to solve this problem?

Thank you.

Niloy

attachments.zip
Parents
  • Hi Jino,

    I am designing a biosensor which detects particle by sensing change in resistance thus change in input current. My normal sensor resistance is 242100/n ohm where n ranges from 1 to 20. Resistance change due to passing particle is in the range 1 to 300 ohm. This change in resistance will be superimposed on to my original sensor resistance. Small change in resistor causes small change in current. My feedback resistance needs to be very high so that I can get a reasonable amplification at the output and detect the change. Also amplifier noise needs to be very low. I hope it answers your question.

    What is your suggestion?

    Thanks.

    Niloy.

Reply
  • Hi Jino,

    I am designing a biosensor which detects particle by sensing change in resistance thus change in input current. My normal sensor resistance is 242100/n ohm where n ranges from 1 to 20. Resistance change due to passing particle is in the range 1 to 300 ohm. This change in resistance will be superimposed on to my original sensor resistance. Small change in resistor causes small change in current. My feedback resistance needs to be very high so that I can get a reasonable amplification at the output and detect the change. Also amplifier noise needs to be very low. I hope it answers your question.

    What is your suggestion?

    Thanks.

    Niloy.

Children
No Data