Is there any information out there for the LET threshold for the AD8561S? Thanks in advance...
AD8561S
Production
The AD8561 is a single 7 ns comparator with separate input and output sections. Separate supplies enable the input stage to be operated from ±5 V dual...
Datasheet
AD8561S on Analog.com
Is there any information out there for the LET threshold for the AD8561S? Thanks in advance...
I am actually looking for the single event latchup rating for the AD8561S. Sorry in advance for the confusion.
Are you asking about the Latch Enable Threshold? On the commercial data sheet,
it has Logic high greater than 2.0V and logic low less than 0.8V.
Threshold typically about 1.6V-1.65V at room.
Harry
Mil/Aero guy says they have no data on the part.
Harry
HARRY,
CHDJ75 ASKED ABOUT SINGLE EVENT EFFECTS LATCHUP RADIATION HARDNESS. I HAVE THE SAME QUESTION. DID ADI OR A 3RD PARTY PERFORM SEL/SET TESTS ON THE AD8561S AND HOW MANY MEV*CM**2/MG IS IT RATED FOR?
No data available.
Harry