Post Go back to editing

AD8672 is very easy to be damaged

I already destroy more then 10 pcs AD8672 in my experiment.

I just use it as a low noise unit gain buffer.

Supply voltage are +/-12V

IN+ is connected to the reference output from LM399.
IN- and output is shorted to provide the negative supply voltage of AD5541.

But I found that the IN+ will follow the negative supply voltage ( ie, -12V ) in my PCB.

Can any one give me the advice?

Parents
  • FormerMember
    0 FormerMember
on Jun 9, 2015 8:21 PM

Tina,

  That's strange.  I would have suspected IC11.

The only thing I can think of would be power supply sequencing issues.

Put a 1k resistor in series with each non-inverting input.

R37 will probably have to be lower.

Harry


Reply
  • FormerMember
    0 FormerMember
on Jun 9, 2015 8:21 PM

Tina,

  That's strange.  I would have suspected IC11.

The only thing I can think of would be power supply sequencing issues.

Put a 1k resistor in series with each non-inverting input.

R37 will probably have to be lower.

Harry


Children
No Data