Protecting the inputs of the ADA4895-1

The ADA4895-1 datasheet lists the maximum differential input voltage to +/-0.7V and that the differential current should be limited to 10mA. In the non-inverting mode for a gain of 10x the recommended resistors are Rfb = 226, Rg = 25.5. If the input can be as high as 5V the total resistance from the input though the to Rg to ground would need to be 500 ohms. With Rg = 25.5 ohms the input resistor would need to be 475 ohms.

Is there a different/better way to insure the input current is limited to 10mA?

Note: The 5V input is the input clamp voltage not the normal operating input voltage.

Scott