Post Go back to editing

ad736 Input range

I´m using AD736 to read RMS value from a shunt resistor in a current sensor. In this case, the 220VAC is fired with a triac, so, the sine wave form is not complete (phase angle control). Using an arduino, which allow 5VDC in its analog ports, my question is: What is the input volts limit from current sensor to AD736 and what will be the max output voltage ? In the datasheet, i´m not sure if it is 1V or 2,7V the limit for input voltage.

Parents Reply Children
No Data