Post Go back to editing

ADA4096 not clamping input in unity gain buffer test circuit

I'm testing the ADA4096-2 amplifier. The testing circuit is an unity gain buffer with a 30Hz sine signal, with dual +/- 3V supply, both amplifiers receive the same signal. I see the output is clamped correctly to the supply voltage values, however, as I increase the amplitude of the signal (>4V above the positive rail), the positive clamping starts to fail and the voltage in the positive power supply rail starts to raise. I'm attaching the image of the test circuit and the signals we are seeing (the red trace is the source signal, the yellow one is the amplifier output).

Am I doing anything wrong? I expected the clamping to work up to 32 V above and below the power rails and not to affect the power rails at all.

attachments.zip
Parents
  • FormerMember
    0 FormerMember
on Jan 30, 2017 11:55 PM

Mario,

  You could put a resistor on the LDO so it sinks 50-100 mA.

Then repeat the experiment.  If you can go higher in input voltage

before the Vdd buss and output start rising, then that would confirm my hypothesis.

Harry

Reply
  • FormerMember
    0 FormerMember
on Jan 30, 2017 11:55 PM

Mario,

  You could put a resistor on the LDO so it sinks 50-100 mA.

Then repeat the experiment.  If you can go higher in input voltage

before the Vdd buss and output start rising, then that would confirm my hypothesis.

Harry

Children
No Data