AD8606
Production
The AD8605, AD8606, and AD8608 are single, dual, and quad rail-to-rail input and output, single-supply amplifiers. They feature very low offset voltage...
Datasheet
AD8606 on Analog.com
AD823A
Production
The AD823A is a dual precision, 17 MHz, JFET input op amp manufactured in the extra fast complementary bipolar (XFCB) process. The AD823A can operate from...
Datasheet
AD823A on Analog.com
Hi,
Could you please provide the AD8606 bias current vs. the common mode for 5V?
For example, here's figure 11 from the AD823A specs:
Thanks for your help,
Keep making these excellent OPAMPs!
Noam
Hi Harry,
Worst cases shown in the table is specify for CM=VCC/2 as states in the table header.
AD8606 is specify as I/O R2R OPA meaning that I can work close to each of the rails. It quite suspicious that Analog-Devices omit Ibias vs CM while giving this info for all other R2R iput OPA I know of...
Noam
Hi Harry,
As I've wrote before:
Worst cases shown in the table is specify for CM=VCC/2 as stated in the table header.
Usually due to ESD diodes and other effects, bias current is higher for CM close to rails.
So I repeat my question again... could you please provide the bias vs. CM voltage or at least specify what's the expected bias current when CM equal to VSS or VCC...
Please help me...
Noam
Noam, we have looked for the data in our archive but it is not available. We agree the graph is useful, and may add it in the future. Yes, the bias current will be higher when the Vcm in near the rails as well as higher variability with temperature and part-to-part.
If you need bias current within ~pA range over the full operating range, please use a lower bias current part, the ADA4530-1 for example. Thank you!
We will be collecting the Ibias vs.Vcm data for the AD8606 and it may take some time. I will let you know once it is available. Thank you for your patience!
Thanks for your help.
I really like to stay with the AD8606 and pay 10% than the superior ADA4530-1.
More profits to me... less to ADI :-)
Thanks,
Noam